hi,we use TJA1100 to design ethercat slave with ET1100,but it is not work . I want to know that it is support this application?
Hi
What function do you want to achieve about TJA1100 in your system?
The TJA1100 is a 100BASE-T1 compliant Ethernet PHY optimized for automotive use
cases.
The device provides 100 Mbit/s transmit and receive capability over a single
Unshielded Twisted Pair (UTP) cable, supporting a cable length of up to at least 15 m.
Optimized for automotive use cases such as IP camera links, driver assistance systems
and back-bone networks, the TJA1100 has been designed to minimize power
consumption and system costs, while still providing the robustness required for
automotive use cases.
I want to use ethercat(TJA1100+ET1100), TJA1100 as a phy in this application,but i don't know Tja1100 which is support this ?
We don't know too much ET1100,please also check your system basic specification also meet TJA1100 before use it.