TJA1100 Master/Slave auto-configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1100 Master/Slave auto-configuration

851 Views
aermakov
Contributor II

Does TJA1100 supports Master/Slave auto-configuration?

If so, how do I set it up?

 
0 Kudos
4 Replies

834 Views
aermakov
Contributor II

is this mean I should periodically switch master-slave programmatically and check if link is up?

Is there way to find out if cable was plugged in case of master/slave mode is not correct, ex. my device is slave and remote device is slave?

0 Kudos

835 Views
aermakov
Contributor II

is this mean I should periodically switch master-slave programmatically and check if link is up?

Is there way to find out if cable was plugged in case of master/slave mode is not correct, ex. my device is slave and remote device is slave?

 
0 Kudos

812 Views
Bulat
NXP Employee
NXP Employee

Normally the automotive ethernet PHYs are used  in pre-defined HW configurations where master-slave roles are known by design. Yes, you can switch master-slave modes periodically and check if link is up.

The PHY has a feature to check cabling errors like open/short, this can be used to test if a remote parter is connected at the cable end.

Regards,

Bulat

 

0 Kudos

848 Views
Bulat
NXP Employee
NXP Employee

No, it doesn't. The user needs to explicitly set the TJA1100 to be a master or slave.

 

Regards,

Bulat

 

 

0 Kudos