Hi,
Schneider Electric is asking what the suffix of /1U versus /1J means on the following:
- TJA1051T/3/1U
- TJA1051T/3/1J
What are the delta's? Do you do a general order as TJA1051T/3 or do you have to include one of the suffixes a the end of the part number, the /1U or /1J?
In the data sheet, the ordering information has on the TJA1051T/3 as an ordering code.
Thanks,
Mike
Hi Tomas
I have a similar question: What does the number "1" mean? I'm looking for the closest replacement type for the TJA1051T/3/1J because it is on status "Not recommended for new designs". The datasheet doesn't tell me anything about suffixes.
Regards,
Marno
Hi Mike,
The only difference is in packaging:
TJA1051T/3/1J – Reel 13" Q1/T1
TJA1051T/3/1U – Bulk Pack
Best regards,
Tomas