TJA1044T/1Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1044T/1Z

738 Views
jiangzz
Contributor II

What's the difference between tja1044t / 1z and tja1044t, 118?

Tags (1)
0 Kudos
1 Reply

728 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

There is no technical difference between them.

The TJA1044T,118 (12NC: 935297572118) is a dual source type meaning diffusion is performed by ICN8 Nijmegen or SSMC Singapore and assembly/test is done done at the NXP Bangkok Thailand facility.

The TJA1044T/1Z (12NC: 935307168431) is a quad source type meaning diffusion is performed by ICN8 Nijmegen or SSMC Singapore and assembly/test can be done either at the NXP Bangkok Thailand facility or at ASE Suzhou China.

If you need a detailed information about the marking for both the TJA1044T,118 and TJA1044T/1Z, please create a standard ticket/case.

Best regards,

Tomas

0 Kudos