TJA1044GT Blockdiagram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1044GT Blockdiagram

400 Views
wenfengyao
Contributor II

About TJA1044GT, is there any imformation introduced VIO and VCC?

How are they connected internally?

wenfengyao_1-1661405018086.png

 

 

0 Kudos
3 Replies

397 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jacky,

Pin VIO is connected to the microcontroller supply voltage to provide the proper voltage reference for the input threshold of digital input pins and for the HIGH voltage of digital outputs. It defines the ratiometric digital input threshold for interface pins TXD, STB and S and the HIGH-level output voltage for RXD. Both the TJA1057/3 and TJA1044/3 provide a continuous level adaptation from as low as 2.95V to 5.25V.

In general, for a full flexibility between 5V and 3.3V applications it is recommended to use the variants with VIO pin.

Best regards,

Tomas

0 Kudos

395 Views
wenfengyao
Contributor II

Hi,Tomas

Can VIO be connected directly to VCC if I am not using STB pin? Will there be any bad effects?

0 Kudos

392 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jacky,

Yes, it can if it is acceptable to the uC TXD and RXD pins.  

Best regards,

Tomas

0 Kudos