TJA1043T是否可以实现NMEA 2000功能?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1043T是否可以实现NMEA 2000功能?

2,132 Views
pengluo
Contributor III

NMEA 2000确认(需要通过NMEA 2000认证):

  目前有款船载机项目,需要支持NMEA 2000功能(根据资料NMEA 2000CAN差不多,但协议不同),帮忙确认如下?

  1.TJA1043T是否可以实现NMEA 2000功能?

  2.供电电压范围和电流范围分别是多少(接口定义如下)?

  3.电源部分是否必须要隔离电路隔离(如下电路)?

 

NMEA 2000扩展资料如下(供参考):

  1.NMEA 2000是船舶工业中常用的通信协议。它允许来自不同制造商的设备无缝协作,从而提高与现有系统的互操作性和集成。

  2.它们通常是五针连接器,分别对应NMEA 2000协议的五个线路:CAN HighCAN LowPowerGround,和Shield。这些连接器可能是微型或中型,具体取决于设备和安装的需求。

  3.NMEA 2000使用最初为汽车行业设计的控制器局域网(CAN)技术。NMEA 2000基于SAE J1939高级协议构建,但使用自己的消息传递方案。

  4.NMEA 2000是NMEA 0183串行数据总线标准的更新版本。与NMEA 0183相比,NMEA 2000的数据速率明显更高(250k /秒对 4800 /秒)。因此NMEA 2000为船舶提供了更好的性能和更可靠的通信。

 

pengluo_0-1725502580872.jpeg

 

pengluo_1-1725502580881.jpeg

 

 

 

Tags (1)
0 Kudos
Reply
1 Reply

2,122 Views
pengluo
Contributor III

我已经获悉:TJA1043可实现CAN部分的功能,其它部分要根据客户的要求来做

0 Kudos
Reply