TJA1042T,118 and TJA1042T/1J

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1042T,118 and TJA1042T/1J

2,301 Views
Chenhaohao1
Contributor II
  • I would to know the difference between TJA1042T,118 and TJA1042T/1J;

2 Replies

2,290 Views
Chenhaohao1
Contributor II

/1J” is used to identify this device as the dual source version of the device. We internally manufacture this device at two FAB locations in order to give our end customer built in dual sourcing for many of our devices. This code is used for the EDI ordering only so there is no technical reason behind. 

1,980 Views
Stanni
Contributor I

Had a look into the Q files and see there is a light difference in the content spec. Bonding wires differs as the weight of the die....and if weight of die differs ...any change in front end process?

0 Kudos
Reply