TJA1040 Date and Batch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1040 Date and Batch

1,105 Views
camerons
Contributor I

Hello,

I have a number of TJA1040 ICs and am wondering if there is a way to determine the batch number and date from the printing on the IC. For instance, one of the chips has the following printing:

A1040/C

DMQ000

nD734

What does the lettering on the chip mean?

Thanks!

0 Kudos
3 Replies

1,054 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Cameron,

I have just received an answer from the application engineer. Please see the description.

DESCRIPTION

The below device date code is actually 2017 week 34, the center line is traceability information and contains wafer and lot information.

A1040/C-(Part number)
DMQ000-
(?)
nD734-
(n=Bangkok   D=Dark Green   7=year 2007 34=week in the year)

The below device marking looks similar to engineering sample coding or earlier silicon version. The /C version of the device was not available until 2014.


A1040/C-
(Part number)
170000-
(?)
D9821-
(D=Dark Green  9=?  8=year 2008  21=week in the year)

Is it possible to get an image of the top of the device? With this, I can verify with this information

With Best Regards,

Jozef

0 Kudos

694 Views
weiqi
Contributor I

hello

we bought some TJA1040 ic 1 month ago, but we can't confirm whether it's true or not. 

the printing on the top of the ic is"TJA1040 0142 nG012" , can you help us to confirm the printing is true or not ?

@JozefKozon 

thanks a lot

0 Kudos

1,054 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Cameron,

could you please provide the Annual Volume? Its not stated in the case.

With Best Regards,

Jozef

0 Kudos