TJA1028TK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1028TK

572 Views
Nihplodic
Contributor I

What is the difference between these two suffixes?

TJA1028TK/5V0/20/1    and 

TJA1028TK/5V0/20/2

Anyone?

0 Kudos
2 Replies

568 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jacky,

TJA1028TK/5V0/20/2 is not an orderable part number, it seems to be a typo.

If you meant TJA1028TK/5V0/20/J, then the packing type (tape & reel 13 inch) is identical with the TJA1028TK/5V0/20,1.

The only non-technical difference is that /J indicates our dual sourced device. This is to help protect from supply chain interruptions that could occur due to natural disasters. 

Best regards,

Tomas

0 Kudos

560 Views
Nihplodic
Contributor I

Thanks Toby,

Requesting a picture of the label from vendor...

0 Kudos