TFA9879 DRC status available?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TFA9879 DRC status available?

385 Views
sergemuller
Contributor I

Hello,

I'd like to indicate to the end user that the DRC (Dynamic Range Compressor) is currently active. I can't find anything that allow me to read directly in the status register anything about that. Did I miss something? In case there's no way to easily get this information, have some of you already figured out a solution to that kind of problem?

Thanks in advance,

Serge

Tags (1)
0 Kudos
1 Reply

349 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Serge,

See below. Reading bit DRC_BP (Reg0Fh[1]) you can see whether the DRC is active or bypassed.

This bit also needs to be set by the user, so it is not a status bit.

 

Dynamic range.jpg

 

Or do you mean you would like to see whether the DRC is ON/OFF during audio playback?

So meaning a status bit that continuously toggles between 1/0 during audio playback ?

This status bit the TFA9879 does not have.

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 Kudos