使用FS8430芯片的BULK2输出1.8V,使用TPS7A8101-Q1将1.8V换换成1.1V作为TEF8102的1.1V_FS电源,TEF8102的1.1V和1.8V供电参考验证版设计,使用PHPT60603NY,集电极采用2.3V供电,2.3V使用FS8430的BULK3产生。TEF8102的3.3V使用FS8430的LDO1产生。目前1.1V、1.8V、2.3V和3.3V都正常,FS8430的BULK2输出的1.8V也正常,只是TPS7A8101-Q1输出的1.1V_FS=0V。如果使用3.3V飞线作为TPS7A8101-Q1的输入,则会有1.1V_FS产生。
如果你不使用PHPT60603NY方案进行供电,而是采取其他方案例如外部LDO、DCDC等(你现在的方案就是其中之一),即便你供电没问题在后续自检过程中也会随机的出现其他问题(这个你可以自行验证)。
上电时序是:1.1V_FS---->1.8V(FS8430 BULK2)---->3.3V
HI
TPS7A8101-Q1 is not NXP products. Can you double check the TPS7A8101-Q1 application circuit?
From 1.045V to 1.155V for FS power.
Hi,
What is the supply voltage range of 1.1V_FS?