TEA2017AAT and TEA2016AAT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA2017AAT and TEA2016AAT

Jump to solution
525 Views
arvind702302
Contributor II

Hi NXP Team,

 

What is the difference between TEA2017AAT and TEA2016AAT?

Thanks.

0 Kudos
Reply
1 Solution
470 Views
arvind702302
Contributor II
Hi Pavla,

And one more doubt Regarding SUPIC Pin - What is exact functionlity of this pin?

I can see this statement in datasheet "When start-up is complete and the LLC controller is operating, the LLC transformer auxiliary winding supplies the SUPIC pin. In this operational state, the HV start-up source is disabled."  Do we need to connect SUPIC pin to Aux winding? What happens if will not connect?

Regards,

Arvind

View solution in original post

0 Kudos
Reply
4 Replies
428 Views
pavla_hajna
NXP TechSupport
NXP TechSupport

Hello Arvind,

for your additional questions I have open another ticket so the responsible engineering team can follow up with you directly.

Have a nice day. Best regards

Pavla

0 Kudos
Reply
485 Views
pavla_hajna
NXP TechSupport
NXP TechSupport

Hello Arvind,

TEA2017 and TEA2016 are pin to pin compatible. 

1. you can replace directly, but because the TEA2017 PFC control is average current mode, so the TEA2017 layout check IC pin 4 GND pin need sense near PFC current Res GND (PFC current sense Res also near the Bulk cap GND) as well. When you replace TEA2017 to TEA2016 board need check about the PFC current operation stable or not. If ok than fine. 

2. For the TEA2016 and TEA2017 programming pin is not same, so when you replace the TEA2017, you need to change the programming pin as attached.

 

3. For the mif setting (software setting) is not same the Ringo tool also not same, the TEA2016 (PFC default is DCM/QR) and TEA2017 (PFC default is DCM /QR /CCM). The PFC control behavior is not same  LLC setting is similar, so confirm with your customer as well. 

Hope this helps. Have a nice day.

Best regards

Pavla

0 Kudos
Reply
472 Views
arvind702302
Contributor II

Hi Pavla,

Thanks for your reply.

Which IC we should use? Which one is latest one?

 

Regards,

Arvind

0 Kudos
Reply
471 Views
arvind702302
Contributor II
Hi Pavla,

And one more doubt Regarding SUPIC Pin - What is exact functionlity of this pin?

I can see this statement in datasheet "When start-up is complete and the LLC controller is operating, the LLC transformer auxiliary winding supplies the SUPIC pin. In this operational state, the HV start-up source is disabled."  Do we need to connect SUPIC pin to Aux winding? What happens if will not connect?

Regards,

Arvind
0 Kudos
Reply