TEA1716T与TEA1713兼容吗?是否可以直接用TEA1716T替换250W电路中的TEA1713,不改变电路?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA1716T与TEA1713兼容吗?是否可以直接用TEA1716T替换250W电路中的TEA1713,不改变电路?

2,195 Views
yangpengyw
Contributor I

我在官网TEA1716T查到的250W用户文档资料里是TEA1713,里面的电路是否把TEA1713换成TEA1716就可以了?

0 Kudos
Reply
5 Replies

1,462 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

I am not sure if I correctly understood your question, but the TEA1713 is pin-to-pin compatible with TEA1716 and is more suitable for applications that do not have severe requirements on burst mode operation and do not require a very low standby power consumption.

Best regards,

Tomas

 

0 Kudos
Reply

1,462 Views
yangpengyw
Contributor I

I'd like to use 1716 to do a 250 W switching power supply.The circuit diagram is made of 1713 which in the NXP website user guide.Can I use this circuit by change nothing except 1713?

0 Kudos
Reply

1,462 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

Yes, you can simply replace the TEA1713 by TEA1716 without any other modifications.

Best regards,

Tomas

0 Kudos
Reply

1,462 Views
yangpengyw
Contributor I

Where can i buy LP3925 and QP-3325? 

0 Kudos
Reply

1,462 Views
yangpengyw
Contributor I

i would be very grateful if you could give me a TEA1713 250 W demo board.

0 Kudos
Reply