TDA8754 as a regular 270Msps ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TDA8754 as a regular 270Msps ADC

729 Views
mmm5651
Contributor I

The TDA8754 is a video ADC IC, with a 270 Msps rate which is pretty good for the price it is being sold at the moment, and I'm working on my final year project which involves a high-speed ADC, and this IC could really fit in if I can make use of it.

So the question is:

Can this IC be used as a regular free-running ADC, without using the sync and clamp capabilities?

Is there any open-hardware project using this IC? The only thing I was able to find was the TDA8754 Demoboard (AN/10295_1)

 

Thanks in advance.

Tags (3)
0 Kudos
Reply
1 Reply

700 Views
nxf45548
NXP Employee
NXP Employee

Dear Mahdi,

Thank you for contacting NXP technical support. 
Following your inquiry, as TDA8754 is an obsolete product, we cannot provide support, as we delete all the documentation related to it. 
I apologize for the inconvenience this may cause you. 

Regards, 
Technical support