T2080 SerDes1_LNnGCR0 PROTS field

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 SerDes1_LNnGCR0 PROTS field

514 Views
scottgerhold
Contributor IV

In the T2080 Ref Manual, Rev 4, 04/2021 the PROTS field (bits 20:24) in SerDesx_LNnGCR0 in section 19.4.18 is defined for some options but not all. We have SRDS_PRTCL_S1 in the RCW set to 0x66, so lane 3 (D) is configured for XFI. The SerDes1_LN3GCR0[PROTS] field is reporting 01010 which isn't defined in the Reference Manual. But the reference manual doesn't define what XFI should report in the  PROTS field. Please let us know what the value should be when the lane is configured for XFI.

0 Kudos
Reply
1 Reply

497 Views
Oswalag
NXP TechSupport
NXP TechSupport

The value "01010'' for SerDes1_LN3GCR0[PROTS] is correct for XFI 10GBase-KR

Regards,

Oswaldo.

0 Kudos
Reply