T1024 DDR3L EOL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 DDR3L EOL

877 Views
kojimiura
Contributor I

I used MT41K512M16HA-125IT (DDR3L) as 600MHz (1200MT/s date rate) for 1024NXN7PQA (CPU) and it works without any problem.
If DDR3L becomes MT41K512M16VRP-107IT: P, can you handle it?
If it can be handled, can the program be used as it is?
Or is it necessary to change the configuration settings of the DDR controller?
Thank you.

0 Kudos
Reply
2 Replies

870 Views
ufedor
NXP Employee
NXP Employee

I believe that the same DDR controller settings can be used for the MT41K512M16VRP-107IT: P.

0 Kudos
Reply

867 Views
kojimiura
Contributor I

thank you for your answer.

0 Kudos
Reply