Spice Model Files For BFU768F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Spice Model Files For BFU768F

ソリューションへジャンプ
1,777件の閲覧回数
derekdszymanski
Contributor I

I'm looking for access to Spice files for BFU768F. Is this something the company will provide? If not, which Spice model should be used to calculate the correct characteristics for this part using the datasheet entries? Are there any other tools that can be used to extract the values for the model?

0 件の賞賛
返信
1 解決策
1,717件の閲覧回数
LPP
NXP Employee
NXP Employee

BFU768F is a variance of BFU760F (selection optimized to operate at 10.8mA). You can use models for BFU760F to simulate BFU768F design.

BFU760F SPICE and MEXTRAM models are provided as a parts of NXP RF small signal kit for Keysight ADS tool.
https://www.nxp.com/products/rf/rf-discrete-components-low-power/rf-wideband-transistors/6-18-ghz-wi...

Also, you can find BFU760F S-parameters on it's web page:
https://www.nxp.com/products/rf/rf-discrete-components-low-power/rf-wideband-transistors/6-18-ghz-wi...

Note, BFU760F SPICE model is available on NXP site: https://www.nxp.com/downloads/en/spice-model/BFU760F.prm
Unfortunately, the quality of the SPICE model is poor and it doesn't match measured RF performance.

My suggestion for you is to use BFU760F SPICE model for DC simulation and S-parameters for RF design.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,717件の閲覧回数
derekdszymanski
Contributor I

Thank you for your help.

0 件の賞賛
返信
1,718件の閲覧回数
LPP
NXP Employee
NXP Employee

BFU768F is a variance of BFU760F (selection optimized to operate at 10.8mA). You can use models for BFU760F to simulate BFU768F design.

BFU760F SPICE and MEXTRAM models are provided as a parts of NXP RF small signal kit for Keysight ADS tool.
https://www.nxp.com/products/rf/rf-discrete-components-low-power/rf-wideband-transistors/6-18-ghz-wi...

Also, you can find BFU760F S-parameters on it's web page:
https://www.nxp.com/products/rf/rf-discrete-components-low-power/rf-wideband-transistors/6-18-ghz-wi...

Note, BFU760F SPICE model is available on NXP site: https://www.nxp.com/downloads/en/spice-model/BFU760F.prm
Unfortunately, the quality of the SPICE model is poor and it doesn't match measured RF performance.

My suggestion for you is to use BFU760F SPICE model for DC simulation and S-parameters for RF design.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信