SYS_MCLK of SGTL5000

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SYS_MCLK of SGTL5000

89 Views
GSXR100038
Contributor II

I would like to know I have to configure the PLL internal to the CODEC or not ? After the DS SYS_MCLK.png

what does that mean ? If my microprocessor can generate a synchronous clock in this case I don't need to configure the PLL of the CODEC, right ? Otherwise I have to configure the registers according to this flowchart ?

PLL.png

Thank you for your answer.

Regards

0 Kudos
1 Reply

70 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

 

If you are using a synchronous SYS_MCLK input from a host processor, you don't need to configure PLL registers since it is not used.

 

You can check an example on section "PLL Configuration" of datasheet.

 

Best regards.

0 Kudos