Hi,
I am interfacing TI TUSS7740 with the i.MX93 FRDM board, the TUSS communicates over SPI
I connected the TUSS SPI to the imx93 LPSPI 3 according to the FRDM schematics:
The DTS node:
What am I missing?
BR
Solved! Go to Solution.
Hi @BaselHn
Yes, you are right: pinctrl-assert-gpios = <&pcal6408 0 GPIO_ACTIVE_HIGH>; in DTS activates the SPI3 to Wi-Fi PHY level converter。
You can remove it from the dts file.
B.R
Hi @BaselHn
Yes, you are right: pinctrl-assert-gpios = <&pcal6408 0 GPIO_ACTIVE_HIGH>; in DTS activates the SPI3 to Wi-Fi PHY level converter。
You can remove it from the dts file.
B.R
hI @BaselHn
You mean this level shifter? It seems from 3.3V to 1.8V, you disconnect the R2797 R2799 R2801 R2805, then resolve the problem?
B.R
Hi @pengyong_zhang
Yes, I also disconnected R2810, R2813, R2815, and R2817. Then it solved the problem.
But when I took another look at the schematics, I think the problem lies in the DTS here :
The SPI3_SW_EN is connected to :
Which is defined in the DTS :). I think the problem has stood since the Tuss tries to raise the line to 3.3 volts and the level shifter makes it 1.2 volts, because of the misconfiguration in the DTS, which enables the level shifter to the MAYA wi-fi PHY.
Can you confirm this?
BR
Basel
HI @BaselHn
You need to run the tset code by yourself, make the spi deive send the data to your master, the you can see the data on the MISO.
You mentioned : I see the data with the logic analyzer, but I did not receive the data on the SOC side.
>>> Could you share your test method and the test result. Include the logic analyzer and log file
Hi @pengyong_zhang
I tried to run the test from the terminal:
pidev_test -D /dev/spidev0.0 -s 500000 -b 8 -H -p "\xBA\x00" -v
spi mode: 0x1
bits per word: 8
max speed: 500000 Hz (500 kHz)
TX | BA 00 __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ |..|
RX | 00 00 __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ __ |..|
Also, I tried to run this C code :
#include <stdio.h>
#include <stdint.h>
#include <fcntl.h>
#include <unistd.h>
#include <sys/ioctl.h>
#include <linux/spi/spidev.h>
#include <string.h>
#include <errno.h>
int main() {
int fd = open("/dev/spidev0.0", O_RDWR);
if (fd < 0) {
perror("open");
return 1;
}
uint8_t mode = SPI_MODE_1;
uint8_t bits = 8;
uint32_t speed = 500000;
if (ioctl(fd, SPI_IOC_WR_MODE, &mode) < 0 ||
ioctl(fd, SPI_IOC_WR_BITS_PER_WORD, &bits) < 0 ||
ioctl(fd, SPI_IOC_WR_MAX_SPEED_HZ, &speed) < 0) {
perror("SPI setup");
close(fd);
return 1;
}
uint8_t tx[2] = { 0xBA, 0x00 }; // Example: read reg 0x1D
uint8_t rx[2] = { 0 };
struct spi_ioc_transfer tr = {
.tx_buf = (__u64)(uintptr_t)tx,
.rx_buf = (__u64)(uintptr_t)rx,
.len = 2,
.speed_hz = speed,
.bits_per_word = bits,
.cs_change = 0,
};
int ret = ioctl(fd, SPI_IOC_MESSAGE(1), &tr);
if (ret < 1) {
perror("SPI_IOC_MESSAGE");
close(fd);
return 1;
}
printf("TX: 0x%02X 0x%02X\n", tx[0], tx[1]);
printf("RX: 0x%02X 0x%02X\n", rx[0], rx[1]);
printf("Received Device ID: 0x%02X\n", rx[1]);
close(fd);
return 0;
}
In both, I get the same result. In the following snapshot, you can see the logic analyzer:
Hi @BaselHn
Your spi configuration is right! You need to run the loopback test, then you can see the data on the RX.
B.R