Hello Pavel
thank you for your reply
On the board I'm testing the two RSTs are tied together. Due to the RST loop that i have (PMIC is resetting the SJA because 1.8V is OV), I'm using an second external voltage monitor only on 3.3V which, after 200ms, It releases the RSTs letting startup the board without other any issues.
From oscilloscope, i can see that:
- immediatly after power up PMIC, 1.8V output voltage is preset on VDDIO_MIIx
- with an expoential RC charge, the voltage rises in 100ms to 2.2V without any apparent reason
- as soon after 200ms (and the external voltage monitor release RSTs) the VDDIO_MIIx pass from 2.2V to 1.8 letting start the board without any other issues.
On RMII ports I have two Atheros, for your information the board is very similar to KITVR5510SKTEVM.
I have no Atheros RST management, but doing an experiment with an external wire on Atheros RSTs tied together with SJA RSTs, behavior does not change.
So my question is: considering that I manage the RST as suggested in AH725720, Is it plausible that an uncontrolled voltage flow inside the SJA during reset and it is reflected to VDD rails?
What other precaution should I have taken?
Regards