[SJA1110] SPI driver can not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[SJA1110] SPI driver can not work

3,051 Views
Ethan_L
Contributor III

Hi everyone,

I am a software RD who's working on SJA1110 ethernet switch project.

I am testing the SPI driver on SJA1110, but I can not measure any signal on the oscilloscope even in master or slave mode.

Does anybody have an idea for this?

Is there any example or document about how to use SPI driver?

 

Thanks, Ethan.

0 Kudos
Reply
7 Replies

2,383 Views
Edieyeee
Contributor I

Hello Ethan,have you solve this problem?

0 Kudos
Reply

3,001 Views
kaden
NXP Employee
NXP Employee

Hi Ethan_L, 

so you want to try to configure the switch via SPI from S32G? Did you check the DIP switch settings are in the correct position? 

They should be set to Serial Boot. 

BR

Kevin

0 Kudos
Reply

2,983 Views
Ethan_L
Contributor III

Hi Kevin,

I set the DIP switch to serial boot mode, but still can't measure any signal.(resistance R607, R624)

Is there any example or document about spi?

Thanks,

Ethan.

0 Kudos
Reply

3,028 Views
kaden
NXP Employee
NXP Employee

Hi Ethan_L,

can you provide additional information? Which hardware are you using (NXP reference board or own design), which software (SJA1110SDK)?

BR

Kevin

0 Kudos
Reply

3,020 Views
Ethan_L
Contributor III

Hi Kevin,

I use S32G-VNP-RDB2 EVM and SDK is SJA1110_SDK(version 1.0.1).

I modified the example "switch_config_s32g_vnp_rdb" for testing.

I try to make S32G274 and SJA1110 communicate via SPI, but it doesn't work.

 

Thanks,

Ethan.

0 Kudos
Reply

2,076 Views
Haribadri1989
Contributor II
Hi Ethan, have you solved this problem?
0 Kudos
Reply

2,532 Views
shanlan123
Contributor II
Hi Ethan_L, have you solve this problem?
0 Kudos
Reply