SJA1105EL is Compatible with IPV4 (IP address)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1105EL is Compatible with IPV4 (IP address)

643 Views
vinayakmaggad
Contributor I

hello,

Am using SJA1105EL Ethernet switch is this switch compatible with IPV4 (IP address)

if yes??

how it can be?

do we need to change the Ethernet frame format??

0 Kudos
1 Reply

587 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

not sure if I understand your question correct, but if you are asking if the switch can forward Ethernet frames based on IPv4 address, then answer is no, because Ethernet frame does not contain IPv4 address. Ethernet frame contains MAC address and every L2 switch forwards frames (switches frames) based on MAC address (if we talk about Ethernet protocol). Different protocols uses different ways (for example PPTP - Point-to-point protocol).

IPv4 address is part of IP packet (IP packet header), which is encapsulated into the Ethernet frame (as a data), and L2 switch does not interested in the packet.

Please see the switching process in the link below

Cut-Through and Store-and-Forward Ethernet Switching for Low-Latency Environments - Cisco 

If you have any other questions, please feel free to write me back.

Regards,

Martin

0 Kudos