SJA1105 with BroadR-Reach and 100Base-T PHY

cancel
Showing results for 
Search instead for 
Did you mean: 

SJA1105 with BroadR-Reach and 100Base-T PHY

142 Views
Contributor III

I want to extend my i.MX6 Quad Board with multiple Ethernet ports.

I need in minimum one BroadR-Reach port and one standard 100Base-T Ethernet port. Therefor I thought to take the NXP SJA1105 with a TJA1100 PHY and a KSZ8081 PHY. The SJA1105  should connect over RGMII with the i.MX6Q.

Is it possible to connect Automotiv Ethernet PHY and Ethernet PHY to the SJA1105 in mixture mode? In that constallatoin I also have a mediaconverter between Automotive Ethernet and Ethernet.

Thanks.

0 Kudos
1 Reply

18 Views
NXP TechSupport
NXP TechSupport

Each SJA1105 port is individually configurable for any supported
type of the interface between MAC and PHY. The type of the transmission
media is not visible at the MAC/PHY interface PHY and only depends on the
capabilities of the PHY device(s) you connect to the switch.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos