hi,
i use the sja1105 to designed a ethernet switch.
i reference the SJA1105UM and MPC-LS-VNP-RDB board (SCH-45700).
int the SJA1105UM refer to:
so,i think the VDDIO_MIIX pin only can be supply 2.5V or 3.3V .
But in the MPC-LS-VNP-RDB board (SCH-45700), it show :
the VDDIO_MII4 supply 1.2V.
so , whether have some err in the different doc?
haiyang
best wish.
Solved! Go to Solution.
The SGMII port on SJA1105R/S has two supply domains: 1.2V and 2.5V for analog IO.
The SGMII port on SJA1105R/S has two supply domains: 1.2V and 2.5V for analog IO.