您好,我想通过SJA1105配置时间戳功能,但是使用过滤模式时如果使用
Hi @BravoEven
In order to use timestamping, it's necessary to use frame trapping (this is explained in more detail in the AH1704 (7.3 Timestamping and AVB).
https://www.nxp.com/webapp/Download?colCode=AH1704&location=null
Also please read chapter 7.3.3 1-step and 2-step SYNC frames.
An example for gPTP can be found in chapter 7.6.6 of the respective application hints.
Regards,
Lukas
Hello
now I want to take the egress timestamp of frame to the host port, for example, a PTP sync frame is forwarded from port1 to port0(host port), I can get the ingress time stamp by the META frame, but how can i get the egress timestamp to calculate the resident time?