SGTL5000 : pop when switch Mic -> Line-in

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000 : pop when switch Mic -> Line-in

1,450 Views
victorien
Contributor IV

Hi,

I'm developping a new board with a SGTL5000 audio codec and I have an issue that I can't resolve.

When I switch input from Microphone to Line-in, there is a pop on audio signal. I see this pop on I2S data and it's look to be generate in the ADC (input or output).

Is there someone who know this issue and find a solution ?

Regards

0 Kudos
Reply
2 Replies

1,091 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

The first recommendation would be to set the “SMALL_POP” bit in CHIP_REF_CTRL 0x0028, setting this bit slows down the VAG ramp from ~200 to ~400 ms to reduce the startup pop, but increases the turn on/off time.

 

Another recommendation would be to mute the outputs during the switch between Mic and Line-in to avoid any pops/clicks, the outputs should remain muted during these chip configuration steps.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,091 Views
victorien
Contributor IV

Hi,

I tested this both solutions but they don't eliminate the pop

0 Kudos
Reply