SGTL5000 Lineout Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000 Lineout Problem

1,984 Views
ray_deng1
Contributor III

Dears,

 

I used SGTL5000+i.MX6 to debug voice lineout.  The first time to trigger voice line out may lead to voice very low, then if trigger in less than 5 seconds, the voice line out may work normal. If trigger more than 5 seconds, the same problem may reappear.

Can you please kindly help to advice?

 

BRs,

Ray

Tags (2)
0 Kudos
5 Replies

1,978 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

Can you please share the SGTL5000 configuration? Pleas also confirm if you are using ALSA (Advanced Linux Sound Architecture).

 

Are you using an NXP evaluation board? We want to see if we can reproduce the issue with our boards and check if it could be a linux problem or an issue related to the i.MX, or confirm if it a problem with the SGTL5000 Codec.

 

For the kind of issue you are mentioning, I’m thinking this could be a problem caused by linux if there are too many pending tasks to run.

 

Regards,

Jose

0 Kudos

1,960 Views
ray_deng1
Contributor III

Hi Reyes,

Thanks for your kindly help.

Please check schematics and SGTL5000 configuration attached.

Customer used ALSA, it just run at customer's board, not NXP EVK.

Also, no pending tasks.

 

Can you please kindly help to advice?

 

BRs,

Ray

0 Kudos

1,933 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Ray,

 

From the HW perspective, I don’t see any problem on the schematic. Just please confirm if the ADUDIO_1V8 voltage connected to VDDD pin of the codec is generated from the SGTL5000 device or if is generated by an external regulator. Because of the 100nF capacitor connected in this pin, I’m thinking the voltage is generated by an external regulator, which is correct.

I ask because of the issues with VDDD regulator and why is recommended for new designs to power it externally, you can find the document in the following link: https://www.nxp.com/docs/en/errata/SGTL5000ER.pdf

 

Now, regarding the SW configuration:

 

According to your SSS_CTRL->DAC_SELECT = 0x1 = I2S_IN configuration, you are bypassing DAP and connecting the I2S input directly to the DAC.

 

When I2S IN -> DAC -> LINEOUT route is selected, output Level (when VDDIO and VDDA are 3.3V) is 1.0 Vrms.

 

Power up the digital and Analog interfaces used (I2S_IN and DAC) using the following bits:

* CHIP_DIG_POWER 0x0002

To power up the I2S_IN (I2S_IN_POWERUP - Bit 0) and the DAC (DAC_POWERUP – bit 5)

* CHIP_ANA_POWER 0x0030

To power up the DAC use DAC_POWERUP

 

Some extra configuration is needed in the DAC to complete the setting:

The DAC output has a digital volume control from -90 dB to 0 dB in ~0.5 dB step sizes. The register CHIP_DAC_VOL controls the DAC volume.

The line output has a dedicated gain stage that can be used to adjust the output level. The CHIP_LINE_OUT_VOL controls the line level output gain.

The line outputs also have a dedicated mute that is controlled by the register field CHIP_ANA_CTRL- >MUTE_LO, you need to make sure it is not activated for your application.

 

You can find an example about how to initialize the SGTL5000 in the following link: https://www.nxp.com/docs/en/application-note/AN3663.pdf

 

Regards,

Reyes

0 Kudos

1,882 Views
ray_deng1
Contributor III

Thanks,  Reyes,

We tested with customer, seems the POP voice cannot be avoid only after 400ms delay.

Do you have any advice?

 

BRs,

Ray

0 Kudos

1,866 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Ray,

 

I’m not sure if I understand, are you saying that you can hear the POP noise from the moment you turn-on the Codec, and after a 400ms this noise issue is eliminated?

 

My recommendation would be to set the “SMALL_POP” bit in CHIP_REF_CTRL 0x0028. Setting this bit slows down the VAG ramp from ~200 to ~400 ms to reduce the startup pop/thunk noise.

Take in mind that enabling this bit increases the turn on/off time.

 

Another recommendation to avoid any pops/clicks (spikes), would be to mute the outputs during the chip configuration steps.

 

Regards,

Reyes

0 Kudos