SC18IS602: Issues with Figure 20 in the datasheet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SC18IS602: Issues with Figure 20 in the datasheet

882 次查看
jc1
Contributor I

When looking at the datasheet for SC18IS602 Figure 20 can be confusing given that during the idle state it should the SPI clock as both high and low for both CPOL states.   The question is what is the SPI clock state during idle?   Also is it possible to get the state of the SS outputs on this figure?   This way we can see the timing of the clock select relative to the clock and data.

标记 (1)
0 项奖励
回复
0 回复数