SC18IS602: Issues with Figure 20 in the datasheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC18IS602: Issues with Figure 20 in the datasheet

885 Views
jc1
Contributor I

When looking at the datasheet for SC18IS602 Figure 20 can be confusing given that during the idle state it should the SPI clock as both high and low for both CPOL states.   The question is what is the SPI clock state during idle?   Also is it possible to get the state of the SS outputs on this figure?   This way we can see the timing of the clock select relative to the clock and data.

Tags (1)
0 Kudos
Reply
0 Replies
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----