SC18IM704-EVB, Is it OK to leave GPIO4 and 5 open?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC18IM704-EVB, Is it OK to leave GPIO4 and 5 open?

255 Views
Yuji_M2
Contributor I

On the circuit diagram, it is directly connected to the pin header in a floating state, but when the power is turned on, it should be an input setting, so an undefined value is read.
Is there a risk of destroying the IC due to shoot-through current when reading an undefined value?
Since there is a Schmidt trigger buffer, can I assume that there is no problem with input only?

0 Kudos
Reply
0 Replies