SC16IS7XX Single byte IRQ with FIFO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC16IS7XX Single byte IRQ with FIFO

1,456 Views
Alilium-Engineering
Contributor II

I am seting up the SC16IS750 on a Linux development (Wayland on IMX8MM) and I need to be able to retrieve single bytes from the SC16IS7xx from the communications bus. One of the issues I have is that the standard Linux drivers take so long in requesting the data byte received it has been overwritten before any byte are actually collected on the I2C bus. 

So this setup is FIFO off giving me an IRQ at the end of the first byte. However I don't get a start signal from the Linux SDA line until 900uS after the IRQ, which is why I am losing the data and is obviously a Linux issue). I had the unit working with the FIFO and triggering on four bytes (minimum with the FIFO on), however this isn't any good for the system I am working on as there are a lot of single byte Acknowledges from the connected devices. 

Alilium-Engineering_0-1616075734810.png

White trace is SCL, Orange is SDA and red is the RX recieve. 


So my question is can I have a FIFO and a trigger level of 1 byte?

 

Thanks in advance. 


Glenn Aitchison

 

Tags (1)
0 Kudos
10 Replies

1,430 Views
Alilium-Engineering
Contributor II

Tried to just replacee with the current file and the build is complaining about the mach/*.h files. 

0 Kudos

1,436 Views
Alilium-Engineering
Contributor II

Hi Jozef, thanks for that, I will read through the drivers files to get a better understanding, I am using Yocto to build the Linux kernel, do I just need to replace the SC16IS7xx.c file with the one attached and include the header file in the same directory?

 

Glenn

1,444 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Glen,

could you please test a linux driver attached?

With Best Regards, 

Jozef

0 Kudos

1,413 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Glen,

I would like to contact an application engineer with the issue. But the application engineers require information below. Could you please provide?

Customer: Altilium-engineering

End Customer: ?

End Application: ?

Country: United Kingdom

Annual Volume: ?

 

With Best Regards,

Jozef

0 Kudos

1,410 Views
Alilium-Engineering
Contributor II

Ho Josef, no problem. 

I am contracting for a company called VMS Newco they manufacture Variable Message signs for the Highways Agency as well as Internation transport groups. 

So the final customer for this is VMS Nemwco/ Highways Agency. 

End application is a Variable message sign controller, this contains an imx8mm SOC, Symphony board and 3 off SC16IS750 uarts each. Overall quantity for the highways agency is around 250 imx8mm per annum and 750 SC16IS550. I don't have anythings for the other international clients. 

Best regards

Glenn Aitchison

1,390 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hello Glen,

please see below an answer from an application engineer I have contacted.

DESCRIPTION

The minimum receive interrupt trigger level is 4 bytes. This device does not support one byte receive interrupt trigger level.

With Best Regards, 

Jozef

0 Kudos

1,387 Views
Alilium-Engineering
Contributor II

Hi Jozef, that isn't quite correct. 

The SC16IS7XX will give a single byte interrupt if the FIFO is off. See image attached.

Is the FE saying there is no way to have FIFO on and a single byte interrupt?

Can you try the IMX8MM team and see how I implement the SC16IS7XX driver that you sent in Yocto, I would like to try this as it seems to creat a software buffer and looks like it could be my solution. If I get the I2C timing issues sorted out. 

Glenn

 

0 Kudos

1,380 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Glen,

I have created a new ticket and moved it in iMX box. There is also a reference to this thread. An support representative from the iMX team will answer you here.

With Best Regards,

Jozef

1,365 Views
Alilium-Engineering
Contributor II

Thanks Josef, one quick question, does the SC16IS750 employ clock stretching, one of the forum questions noticed that the clock line is held low during the delay.

 

Best regards

 

Glenn

0 Kudos

1,347 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Glen,

Unfortunately no, SC16IS750 does not support clock stretching.

With Best Regards,

Jozef

0 Kudos