SC16IS741AIPWJ does it supports 115200 baud rate in IrDA communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC16IS741AIPWJ does it supports 115200 baud rate in IrDA communication

Jump to solution
1,077 Views
Rajesh_Kaliyaperumal
Contributor I

Hi Team,

I am trying to figure out whether SC16IS741AIPWJ can be used for the IrDA baud rate of 115200. in the data sheet all i could find out is the table which does not mention about 115200 baud.

 

Rajesh_Kaliyaperumal_0-1662554442500.png

Could you clarify whether 115200 baud rate is supported by this device with prescaler and divisor set to 1 with the 1.8432 MHz clock ?

Appreciate you help at the earliest !

Regards,

Rajesh

0 Kudos
Reply
1 Solution
1,060 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Rajesh,

I think your assumption is totally correct and such baud rate should be supported by both ICs.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
4 Replies
1,070 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Rajesh,

On SC16IS760 IrDA baud rate is supported. Please see the AN10417 about NXP IrDA rates supported by the SC16IS760.

Best regards,

Tomas

0 Kudos
Reply
1,065 Views
Rajesh_Kaliyaperumal
Contributor I

Hi Tomas,

Thanks for you suggestion.

As per the below formula for the divisor in the data sheet, is it possible to get the internal baud rate clock output (16x Desired Baud rate i.e 16*115200 = 1.8432 MHz) from the XTAL1 input clock  (1.8432MHz) as it is by setting the prescaler logic as 1 (by setting MCR[7] =0)  ? 

Rajesh_Kaliyaperumal_0-1662633321070.png

Rajesh_Kaliyaperumal_1-1662633358075.png

if the mentioned logic  is possible , then we can use either SC16IS741AIPWJ or SC16IS760 ? Could you confirm whether my inference is correct ?

 

Regards,

Rajesh

0 Kudos
Reply
1,061 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Rajesh,

I think your assumption is totally correct and such baud rate should be supported by both ICs.

Best regards,

Tomas

0 Kudos
Reply
1,057 Views
Rajesh_Kaliyaperumal
Contributor I

Thanks Tomas,

Will test it out here and let you know if I face any difficulty.

 

Regards,

Rajesh

0 Kudos
Reply