Hello everybody.
Going to offer as carry-over a design running with CAN SBC UJA1169A which is per datasheet compliant to ISO 11898-2:2016 and SAE J2284-1 to J2284-5.
Our customer spec is calling out for the following:
- CAN -J1939-14-2016 12 - Physical layer, 500kbps
- SAE J1939-17 for physical layer
- SAE J1939-22 for transport protocol layer
Does anybody know if SBC standard compliance is fully covering our customer request or if we need to look for different solutions?
Thank you. Kind regards,
Samuele
Hello Samuele,
yes, the UJA1169A will work with the SAE J1939 protocol.
With Best Regards,
Jozef
Hello Jozef and many thanks for your reply and explanation.
Kind regards,
Samuele
Hello Samuele,
you are very welcome.
With Best Regards,
Jozef