S32V234 Boundary Scan Test Enable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32V234 Boundary Scan Test Enable

532 Views
roy_rf
Contributor I

Hello, I'm trying to enable the Bscan Cells for the s32v234, sending the 4'b0110 to the Instruction Register and then the h200_00000000_00000000_00000000_74020000_07003E10 through the Data Register, as is specified in the BSDL, but the Boundary-scan is not working.

I have to do any other step or instruction before or after, to enable the boundary scan test in the ICT?

Here is the instruction for the BSDL.

-- *****************************************************************************
-- BSDL file for design --> s32v234
-- Company --> Freescale Semiconductor
-- Designer --> b37480
-- BSDL file generated on --> 11-Jul-2015
-- Tool --> BSDL_GEN, Version 5.0
-- DESIGN WARNING
-- JTAG Data Register with opcode 4'b0110 need to be programmed to run bscan.
-- Opcode: 4'b0110
-- Data : 170?h200_00000000_00000000_00000000_74020000_07003E10
-- *****************************************************************************

Attached you can find the PCF created to load both registers with the requested data.

0 Kudos
1 Reply

509 Views
andrei_skok
NXP Employee
NXP Employee

Please be informed, that all support to S32V234 is done via tickets. This Community is not appropriate for questions of this kind. Our engineer will answer your questions via opened Support Case.

 

0 Kudos