S32R45:Whether the DDR speed meets the requirements?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R45:Whether the DDR speed meets the requirements?

1,029 Views
Shi_test
Contributor III

Has anyone encountered this problem?

    On the basis of "RSDK_Multi_RFE_example_S32R45" I tried to run 1024-512-16 range with RF and SPT ( The output data format is "CP4Q_FMTA" ) . I found it OK to put the processed data on SRAM. But if i want to put the processed data on DDR it will not succeed. Because SPT does not return the completion callback "SptEcsIsrCb".  So I wonder if it is possible that the DDR speed is not as fast as the SRAM, causing the loss of chirp?

Shi_test_0-1689325795104.png

 

 

 

0 Kudos
Reply
5 Replies

864 Views
WenChao
Contributor II

Hi I have the same quetion as you, dou you have some ideas to solve it?

0 Kudos
Reply

631 Views
Shi_test
Contributor III
官方说不建议将RF+range步骤的输出放到DDR。
0 Kudos
Reply

1,003 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

If the issue is still relevant can you please submit a ticket at NXP.com so I can escalate this to RADAR team?

https://community.nxp.com/t5/HomeTest-Knowledge-Base/How-to-submit-a-new-question-for-NXP-Support/ta...

Best regards,

Peter

0 Kudos
Reply

960 Views
Shi_test
Contributor III

Shi_test_0-1690786995137.png

Hi Peter: 

I did what you wrote,but I don't have access.

What should I do in this case?

0 Kudos
Reply

948 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

What exactly you did? There should be no restriction for ticket submit.

Just to have account created on NXP web.

Best regards,

Peter

Tags (1)
0 Kudos
Reply