S32R41_TEF82XX_DEV_PLATFORM_V1.1 Compile Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R41_TEF82XX_DEV_PLATFORM_V1.1 Compile Error

3,266 Views
longfeiwang
Contributor III

I try to compile S32R41_TEF82XX_DEV_PLATFORM_V1.1, after that I got some errors(My computer is a newly installed system without installing any software unrelated to S32R41_TEF82XX_DEV_PLATFORM_V1.1)。

1 Because I don't have the license of the trial version of bbe32, many errors will appear after I cancel the license, how can I get the license of the trial version?

longfeiwang_0-1691981606369.png

 

2 After compiling S32R41_TEF82_APP_M7_1, it prompts that the file Os_prop.h cannot be found. I searched my hard disk and still can’t find this file. Which update package do I need to install?

longfeiwang_1-1691981619436.png

 

Currently only S32R41_TEF82_APP_M7_0 can be successfully compiled。

Tags (1)
0 Kudos
Reply
7 Replies

3,220 Views
nxf92108
NXP Employee
NXP Employee

Hi,

For question 1, you should contact your radar FAE.

For question 2, you should install S32DS and required packages by following chapter 3.1 Table 1 in S32R41+TEF82xx development platform user manual.

 

0 Kudos
Reply

3,199 Views
longfeiwang
Contributor III

Thanks for the reply。

question 2,:I have installed the required software strictly according to the manual

0 Kudos
Reply

3,191 Views
nxf92108
NXP Employee
NXP Employee

Hi,

The file Os_prop.h is generated by "Generate Configuration" operation and located in generate/rtos/Os_prop.h. You may want to check the file existence first and then check RM chapter 5.5 for build steps.

BR.

0 Kudos
Reply

3,145 Views
longfeiwang
Contributor III

 

All required installation packages have been installed, and the error message is as follows:

System Generator for AUTOSAR OS/S32R41 - Version 4.4.124
EAR Software - NOT FOR PRODUCTION
NXP(TM) and the NXP logo are trademarks of NXP.
All other product or service names are the property of their respective owners.
(C) Freescale Semiconductor, Inc. 2013-2016
Copyright 2022 NXP

D:\S32R41\S32DS\S32R41_TEF82_APP_M7_1\generate\rtos\RTOS_S32R41.ecvd(12) AUTOSAR/AR-PACKAGES/AR-PACKAGE[SHORT-NAME='RTOS_S32R41']/ELEMENTS/ECUC-MODULE-CONFIGURATION-VALUES[SHORT-NAME='Os']/CONTAINERS: error 3254: Multiplicity check error for '/Os/OsAppMode'
d:\S32R41\S32DS\S32R41_TEF82_APP_M7_1\generate\rtos\RTOS_S32R41.ecvd - 1 error(s), 0 warning(s)

0 Kudos
Reply

3,186 Views
longfeiwang
Contributor III

"Generate Configuration" This operation has been operated, and it seems that nothing has been generated.

0 Kudos
Reply

3,164 Views
nxf92108
NXP Employee
NXP Employee

Hi,

Normally "Generate Configuration" will generate files under directory generate/rtos. It looks like you have issue in this step. You should check your installed required software.

 

0 Kudos
Reply

3,256 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

how can I get the license of the trial version?

The BBE32 DSP debugging requires some additional setup beyond the installation of the BBE32 DSP Add-On Package for S32R45. The BBE32 has a different license from the one for S32 Design Studio. This license must be located using the ‘LM_LICENSE_FILE’ environment variable, as instructed within the provided document "{S32DS Install DIR}\Release_Notes\BBE32_DSP_Release_Notes.pdf".

Which update package do I need to install?

Not sure here. It looks like you are missing RTOS package.

Anyway I am escalating this case to the regional FAE, he will take care of it.

Best regards,

Peter

 

0 Kudos
Reply