Hello, I was using the s32r274 radar development board. Until last week, I was able to run demo projects such as RSDK_DEMO, OneRf_4Antennas demo and udp_rtos_project . But even though I didn't make any changes, I got this error and I couldn't solve this problem. I would be happy if you help. (I am using S32DS v2.1)
To solve this problem, I deleted the ide and the drivers connected to the ide and reinstalled it, but the error was not resolved.
Hello,
Ok, and do you see it in your 3.0.3 package?
Best regards,
Peter
Hello,
Yes I can see this file.
Hello,
I have tried to compile OneRF demo with just these installed:
No errors were reported. Since you have PA_15 in your repository, I guess it will be some issue with the installation which I cant reproduce from available information.
You can subscribe ticket to S32DS team at NXP.com if you want to get in touch with SW team.
Best regards,
Peter
Yes I installed SDK 3.0.3 package as you can see the below picture. I could not understand your solution suggestion in the link you added as the link address.
Hello,
Not sure what happen, but do you have installed SDK 3.0.3 package?
SDK_S32_PA_15 is part of it.
See following thread:
Best regards,
Peter