S-parameters (s2p file) for MOSFETs MRF6S20010NR1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S-parameters (s2p file) for MOSFETs MRF6S20010NR1

931 Views
andreysklyuyev
Contributor I

Hello All,

Could you send my S-parameters (s2p file) for MOSFETs MRF6S20010NR1 Freescale Semiconductor?

Thank you

0 Kudos
3 Replies

634 Views
milanbaca
Contributor III

we do not have s2p file.

That part is relatively old, designed in 2005 and it has a newer version that has higher RF performance numbers and a  smaller package.

New designs should utilize the AFT27S0101N in place of the MRF6S20010N, although the 20010nR1 runs in very high volumes and there is no possibility of it going EOL for the next 5 years.

0 Kudos

634 Views
andreysklyuyev
Contributor I

Hi Milan,

Thank you for answer and recommendation. I simulated preliminary design 10W

PA on AFT20S015N in wide band frequency 1.7 - 2.3 GHz.

It is possible receive engineer recommendation/suggestion (layout,

schematic, etc.) for this wide frequency band?

My design shows low S21 = 10 dB and S11= - 2 dB.

Thank you

Regards

Andrey Sklyuyev, Ph.D.,

Senior RF/MW Engineer Alga Microwave

514-694 8666 ext.223

0 Kudos

634 Views
milanbaca
Contributor III

I'm sorry, we do not have designed test circuit for your frequency range.

0 Kudos