Running application from internal SRAM on MPC5554

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Running application from internal SRAM on MPC5554

1,776 Views
dranne
Contributor I

I want to program MPC5554 so that the code finally runs from the internal SRAM i.e. program the flash with the application code and at run time this code runs from the internal SRAM, how to do this.

Any help would be highly appreciated.

 

Thanks in advance.

dranne

0 Kudos
8 Replies

801 Views
dayve
NXP Employee
NXP Employee

Hello Dranne,

 

There is 2 things that need to happen.

1. When the code is compiled the compiler needs to know that this is what you intended to do. Otherwise it will operate relative to the flash address when it does a branch etc rather than the ram that you have moved it to.

2. You need to copy over the code in your flash boot code and point the PC to it once it is all copied.

 

This is a valid thing that you want to do. I am using the Greenhills compiler and it provides an example to do what you ask. I have also done this before in Windriver and I remember that they also described how to do this in their documentation.

 

Regards,

Dayve

0 Kudos

801 Views
dranne
Contributor I

In which of the files, will I have to make these changes.

 

Regards

dranne

0 Kudos

801 Views
dayve
NXP Employee
NXP Employee

Hey Dranne,

 

Have a look in the Codewarrior forum, there are some questions about this topic.

 

Here is a thread that will help you out.

 

https://community.freescale.com/thread/66070

 

Regards,

Dayve

0 Kudos

801 Views
dranne
Contributor I

Thanks Dayve, I'll get back to you on this with more questions.

0 Kudos

801 Views
dranne
Contributor I

Hi Davye

 

I used the sample code in the reference link you emailed.

But when I call the function in main it gives link error

 

 'Link error: Relocation(10) of symbol 'MyFunc' in 'main.o'

is out of range. ...

Link failed.

 

What to do of this? I am using Code Warrior IDE version 5.9.0. Any help would be highly appreciated.

 

Regards

dranne

0 Kudos

801 Views
stanish
NXP Employee
NXP Employee

Hello dranne,

 

This link error is caused by the fact the code in RAM is out of range of PC relative addressing that is used by default.

Therefore I'd suggest you to explicitly specify that far absolute addressing should be used by pragma: e.g.:

 

#pragma push
#pragma section code_type ".my_RAM_code" ".my_
RAM_code" data_mode=far_abs code_mode=far_abs
void myfunc1(void)
{
   ...
}
#pragma pop

 

I hope it will help.

 

Stanish

 

 

0 Kudos

801 Views
dranne
Contributor I

Hi

Yes it helped, thanks will ask more on this.

 

Regards

dranne

0 Kudos

801 Views
dranne
Contributor I

Hi Dayve, Can you please tell me how to do it in Freescale codewarrior. Any sample code may help me a lot.

 

Thanks in advance

 

Regards

dranne

0 Kudos