Hello,
We are having serious problems connecting to a CYT2B95CAC part using SWD and a JLink segger.
This is the message displayed on j-flash
Can you help please?
Thanks
Message :
Connecting ...
- Connecting via USB to probe/ programmer device 0
- Probe/ Programmer firmware: J-Link V11 compiled Dec 7 2021 08:37:18
- Device "CYT2B95CAC_M0" selected.
- ConfigTargetSettings() start
- Disabling flash programming optimizations: Compare, SkipBlankDataOnProg and flash breakpoints
- J-Link script: ConfigTargetSettings()
- ConfigTargetSettings() end
- ConfigTargetSettings() start
- Disabling flash programming optimizations: Compare, SkipBlankDataOnProg and flash breakpoints
- J-Link script: ConfigTargetSettings()
- ConfigTargetSettings() end
- Target interface speed: 200 kHz (Auto)
- VTarget = 3.354V
- ConfigTargetSettings() start
- Disabling flash programming optimizations: Compare, SkipBlankDataOnProg and flash breakpoints
- J-Link script: ConfigTargetSettings()
- ConfigTargetSettings() end
- ConfigTargetSettings() start
- Disabling flash programming optimizations: Compare, SkipBlankDataOnProg and flash breakpoints
- J-Link script: ConfigTargetSettings()
- ConfigTargetSettings() end
- ERROR: Failed to connect.
Could not establish a connection to target.
Regards,
Abdelhadi
yes, Abdelhadi, this is what I can see in your original request, but I am trying to understand why are you asking NXP for help with Infineon product:https://www.infineon.com/cms/en/product/microcontroller/32-bit-traveo-t2g-arm-cortex-microcontroller...
If the problem is with JLink you may need to contact Segger: https://www.segger.com/products/debug-probes/j-link/
Have a nice day
Pavla
yes, this is what I can see in your original request, but I am trying to understand why are you asking NXP support for help with Infineon product:
If the problem is with JLinkk you may need to contact Segger: https://www.segger.com/products/debug-probes/j-link/
Have a nice day
Pavla
Hello Abdelhadi,
what is the NXP part number you refer to? Thank you in advance. Have a nice day. Best regards. Pavla
Hello Pavla,
We work with CYT2B95CAC
Thank you in advance.
Best regards,
Abdelhadi BENTAYEB