Reason for TEA machine check exception

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reason for TEA machine check exception

Jump to solution
2,224 Views
mditto
Contributor I
I am using a custom MPC8248 board running Linux 2.4.  I occasionally get a
machine check exception when trying to read from an address that should be
mapped to PCI space.  The reason is supposedly a transfer error acknowledge
(SRR1=41030).  As far as I can tell from the 8272 reference maual, this means
that the !TEA signal was asserted during the bus cycle, but on this board that
pin is pulled up to VCC.  Is there some other condition that causes a TEA
machine check?

Thanks in advance.

Mike

Tags (1)
0 Kudos
Reply
1 Solution
1,518 Views
mditto
Contributor I
(Answering my own message for anyone interested.)

It seems that TEA is internally asserted by the PCI bridge when it raises a
machine check exception, or at least it fills in SRR1 as if there was a TEA.
The PCI registers, such as PCI_ECCR, can be consulted to get the
details about the PCI bus error in this case.

View solution in original post

0 Kudos
Reply
1 Reply
1,519 Views
mditto
Contributor I
(Answering my own message for anyone interested.)

It seems that TEA is internally asserted by the PCI bridge when it raises a
machine check exception, or at least it fills in SRR1 as if there was a TEA.
The PCI registers, such as PCI_ECCR, can be consulted to get the
details about the PCI bus error in this case.

0 Kudos
Reply