Reason behind CAN Data Bytes limited to 8 bytes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reason behind CAN Data Bytes limited to 8 bytes

449 Views
pranavpathak
Contributor III

Dear all,

Can anyone please explain the reason behind limiting the CAN Data Bytes in a message to 8 bytes, even if length of DLC field is 4 bit which can be used to transmit 16 bytes of data ? Is there any specific reason behind this ? #can frame#can bus#can networks#can driver

Thanks,

Pranav

0 Kudos
0 Replies