Hi,
We are trying load and boot an example GPIO LED program onto an RW612 in ISP Mode using UART.
Currently I can load the code onto the RW612's Flash and exit ISP mode for the code to run.
What I want to achieve is using blhost to load the code onto ram instead of flash and execute it from there.
These are the steps that I'm currently using
If anyone has any ideas that would be great!
Thanks,
Alex
Hi,
I will contact you in the internal case 00651929 to avoid confusion.
Regards,
Daniel.