RT685S, DSP core debugging too slow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT685S, DSP core debugging too slow

1,413 Views
SSFG1992
Contributor I

Hello, I am debugging a dsp demo in Xtensa Xplorer. It takes about 30 seconds to configure GDB while launching jlink. Is it correct? In addtion, It seems not smooth while debugging step by step.1599785371(1).png

It is my debug configuration. Is there any problem with this configuration? Maybe I ignored some other configurations, so please help me configure it correctly. Thanks!

1599786789(1).png

0 Kudos
Reply
2 Replies

1,280 Views
ztzstan
Contributor II

我也是30秒。我尝试了在Ubuntu下安装xtensa和mcuexpresso,build和下载都OK,但是DSP下载速度还是太慢。我抓取了debug口上下载时的波形,发现每下载27us一个packet,就偷懒休息300us。如果没有这300us的偷懒,下载速度可以提高至少5倍!

微信图片_20210820114645.jpg

 this is a problem that NXP must fix! 

0 Kudos
Reply

1,401 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

30 seconds is a bit long. But I think it's fine.  My computer need 20 second to download. I use the default debug configure. It seems the speed is same as your setting.

 

Regards,

Jing

0 Kudos
Reply