RFID CLRC663 Tag authentication issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RFID CLRC663 Tag authentication issue

1,576 Views
Kezi
Contributor I

Hi Team.,

I'm working on CLRC663 Eval board communicated  via SPI with Renesas S7G2 mcu .

Could read ATQA,SAK and UID from ntag213, ntag216 and MIFARE DESFire RFID Tags via ISO1443 with 106kb/s.

 

Now i'm trying to authenticate the tags to write and read data , but unable to do it.

Can you please help me.

 

0 Kudos
Reply
1 Reply

1,548 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Kezi ,

 

The Mifare Desfire demo which contains the authentication process is available in the doc store, but you have to sign the NDA with NXP before fetching this package as below.

Kan_Li_0-1630906337117.png

Please kindly refer to the attachment for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 Kudos
Reply