RF transistor MRFE6VS25NR1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RF transistor MRFE6VS25NR1

589 Views
marcapfel
Contributor I

Hello,  For a project I use the RF transistor MRFE6VS25NR1. According to the datasheet, pin 3 (source) is under the component and connected to ground. When I look the PCB examples, the transistor is placed over a cut out area. The pin 3 seems to be not connected to ground. Can you explain to me why?  Thanks for your help.

0 Kudos
1 Reply

502 Views
LPP
NXP Employee
NXP Employee

The reference design has PCB board bonded to metal pallet carrier.
The leads are soldered to the PCB, and the source contact or the heat spreader is soldered to the carrier.

The carrier should provide low impedance path for heat flow and also low impedance for RF signal.

Please refer to this application note:
https://www.nxp.com/docs/en/application-note/AN1907.pdf

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos