REALTIMEEDGE Version_2.1: several parameters about IEEE 802.1AS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

REALTIMEEDGE Version_2.1: several parameters about IEEE 802.1AS

209件の閲覧回数
Toooong
Contributor II
  1. In 1AS_Automotive Profile mode, how to configure different Sync_interal parameters for each port, which could be modified in /etc/genavb/fgptp-br.cfg ? For example, set swp0 to 62.5ms, set swp1 to 125ms.
  2. How to view Exception Log, such as the timestamp(s) of the Loss of Sync event(s)、Pdelay Response Timeout event、The time of lose of Sync and The time of Pdelay Response Timeout and other parameters. Using commands like "tail -f /var/log/fgptp-b" cannot show the parameters mentioned before.
タグ(3)
0 件の賞賛
0 返答(返信)