R52 PIT is not working RTU's Core1,2 & 3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

R52 PIT is not working RTU's Core1,2 & 3

Jump to solution
295 Views
srinivasulut
Contributor III

I have configured the PIT_0 & PIT_1 to RTU's of core_0 & core_1. for core_0 both PIT_0 & PIT_1 instance are working fine. for core_1 none of the PIT instances are not working. 

when i configure STM for both cores and it is working fine. the PIT is not working.

I am using nxp eval HW for S32N series. The FSS and RTU configurations are done. 

srinivasulut_0-1700587787710.png

srinivasulut_1-1700587908552.png

 

 

0 Kudos
1 Solution
263 Views
srinivasulut
Contributor III

It is working. the issue with GICD configuration in OS side and fixed the same at OS and it is working PIT for all cores.

View solution in original post

0 Kudos
1 Reply
264 Views
srinivasulut
Contributor III

It is working. the issue with GICD configuration in OS side and fixed the same at OS and it is working PIT for all cores.

0 Kudos