Questions about the MAG3100 magnetometer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about the MAG3100 magnetometer

470 Views
heelcurve5
Contributor II

I have several questions regarding the MAG3100 magnetometer. 

1. The spec lists many Output rates  and oversample ratios. What are the use cases? For example when should an output rate of 80Hz be used vs 0.08 Hz? What is the optimal output rate / oversample ratio for an e-compass application?

2. The  part has an option to do triggered measurement, i.e sample once and go into standby, as opposed to continuous sampling in active mode. What is a typical use case for this feature?  Can/should it be used in an e-compass application? 

Thank you

Andy

Tags (1)
0 Kudos
0 Replies