Questions about the KW45B41Z83AFPAR 「BOOT_CONFIG」 pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about the KW45B41Z83AFPAR 「BOOT_CONFIG」 pin

Jump to solution
697 Views
kkobayashi1
Contributor I

For the 「KW45B41Z83AFPAR」, the 「BOOT_CONFIG」 pin is set to Hi at BOOT, but do you need an external pulldown during normal operation?

0 Kudos
Reply
1 Solution
622 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @kkobayashi1 ,

 

We believe that if the BOOT_CONFIG pin is left open (not connected to a defined logic level), it will likely float and transition between high and low voltage levels unpredictably.

So, it should better pull-up or pull-down definitely. 

 

Best regards,

Gavin

View solution in original post

0 Kudos
Reply
3 Replies
656 Views
kkobayashi1
Contributor I

Thank you for your reply.

If the BOOT _ CONFIG pin is Open, will it recognize "H" or "L" at startup?

0 Kudos
Reply
623 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @kkobayashi1 ,

 

We believe that if the BOOT_CONFIG pin is left open (not connected to a defined logic level), it will likely float and transition between high and low voltage levels unpredictably.

So, it should better pull-up or pull-down definitely. 

 

Best regards,

Gavin

0 Kudos
Reply
678 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @kkobayashi1 ,

Thanks for contacting NXP support.

After the board boots, we should keep the [BOOT_CONFIG] pin unchanged, no external pull-down is required.

 

Best regards,

Gavin

0 Kudos
Reply